Change tag values at runtime

If the signed in user has write permissions to a display, objects on the display can change tag values at runtime. When the tag value is changed, a status message indicates whether the tag write completed successfully. If the tag write does not complete successfully, an error message is shown.
TIP:
The status bar appears at the bottom of the display as a default. Click the "x" to close the status bar.
Tag values can be changed using the following graphic objects:
  • Push buttons:
    • Momentary
    • Maintained
    • Multistate
    • Interlocked
    • Ramp
  • String input objects
  • Control list selectors
Push buttons and control list selectors behave identically to their
FactoryTalk View
counterparts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal