Connect to a web application
Connect to a web application to view displays containing information about your plant or process.
If the web application has security enabled and
Remember me on this computer
is selected, FactoryTalk ViewPoint
automatically logs in using the most recently entered username and password. To prevent unauthorized access to the FactoryTalk ViewPoint
server, do not select this option on shared or public computers.To connect to a web application
- Start a web browser.
- In the browser'sAddressbar, enter the desktop or mobile URL, replacingcomputer_name_or_ip_addresswith the hostname or IP address of theFactoryTalk ViewPointserver:
- (desktop)http://computer_name_or_ip_address/FTVP
- (mobile)http://computer_name_or_ip_address/FTVP/m
If the site has an HTTPS binding, enterhttpsinstead ofhttp. - (optional) If the web application has security enabled:
- Enter a username and password.
- (optional) SelectRemember me on this computerto save the sign-in details until the account is signed out, the password expires, or the account is disabled.
- ClickSign in.
Provide Feedback