Analyze data in FactoryTalk ViewPoint trends
A FactoryTalk ViewPoint trend shows real-time or historical pen values from a data server defined in a
FactoryTalk View
trend or trend pro object.Most features of a
FactoryTalk ViewPoint
trend cannot be modified in a web browser at runtime. To change pen definitions or properties, open FactoryTalk View Studio
, modify the original object, and then publish the changes to the web application.Provide Feedback