Configure the X axis
Configure the X axis to change its start date, amount of time shown, or historical data end date. Configuring the X axis pauses the trend.
To configure the X axis
- In theFactoryTalk ViewPointtrend page, selectMenuand then selectX-Axis Rangeto show the Trend Configuration window.
- UnderX-Axis, inStart Date, enter the date on which the trend should start.The start date cannot be earlier than the end date specified underHistorical Data Retrieval.
- InTime Span, enter the number of seconds, minutes, hours or days the trend will show.The default value is the same as the value of time span of theFactoryTalk Viewclient trend or trend pro object.
- UnderHistorical Data Retrieval, inEnd Date, enter the last date for which historical data will be retrieved.
- ClickApplyorOKto save the changes.
Provide Feedback