Select a pen
Select a pen to highlight its line in the trend. The pen increases in width and the Y-axis changes to show the Min and Max values for the pen.
To select a pen
- In the legend, select the pen description.
Provide Feedback