FactoryTalk ViewPoint desktop interface
The desktop interface presents navigation and status information in a compact format suitable for a high resolution computer screen.
By default, the desktop interface scales the selected display to the width of the web browser, regardless of settings specified for the display in
FactoryTalk View Studio
. When displays are scaled, the original aspect ratio is not preserved.FactoryTalk ViewPoint
application using the desktop URL.Provide Feedback