Header bar
Use the header bar to see display permissions, sign out, access help, or view
FactoryTalk ViewPoint
version information.
Item | Description |
|---|---|
![]() | The permissions icon shows which read or write permissions have been granted to the current user. |
![]() | Shows the current user. Click the icon to switch users. |
![]() | Shows Help. |
![]() | Shows FactoryTalk ViewPoint version information. |
Provide Feedback