Disconnect from a web application
Disconnect from a web application to stop viewing displays.
To disconnect from a web application
Use one of these methods:
- Close the browser.
- On the mobile menu, clickSign out.
- On the FactoryTalk ViewPoint Administration Home page, click
. - On the tablet header bar, click
, and then click Sign out.
Provide Feedback