Archive Management of Change website
Administrator has to configure electronic workflow rules for the application. For more
information, see
FactoryTalk AssetCentre Desktop Client Help.
How do I open Archive
Management of Change?
Prerequisites
- Make sure that you have activated Management of Change after installingFactoryTalk AssetCentre.
To open Archive Management of Change
- SelectTools > Management of Change Admin.
FactoryTalk AssetCentre
integrates with Management of Change adding a new level of security of to the existing security available for version control and archive of program files and documents. When installing FactoryTalk AssetCentre, you will be assigned as a Management of Change administrator by default. You can change the security settings to implement the Management of Change workflow for a file, binder, or folder. When you start a check-out or check-in workflow for a file, binder, or folder, other users cannot perform the check-out or check-in operation until the workflow is approved or rejected, or the Unblock Workflow
command is used. Archive Management of Change is a separately licensed and activated capability within FactoryTalk AssetCentre
.Use the Archive Management of Change website to:
- Change request rules
- Manage users
Provide Feedback