Configure conditions
You must configure conditions for the check-in or check-out workflow. Only after you set the conditions, the request will be sent to the approvers.
To configure conditions
- On theChange Request Rulespage, selectCheck OutorCheck In.
- SelectCreate Rule.TheConditionstab opens.
- SelectAdd another Condition.
- In theCreate a condition for type: Change Requestdialog, configureAttribute,Comparator, andValue.For example, you can set them as below:Attribute: Work Order TypeComparator: equal toValue: Check OutForFactoryTalk AssetCentreusers, only theWork Order Typeattribute and itsCheck OutandCheck Invalues are available.
- SelectOK.
- (optional) To create more than one condition, selectAdd another Condition.
- (optional) To create more than one group of conditions, selectOr add another group of Conditions.
- SelectSave.
Provide Feedback