Unblock a Management of Change workflow
When a Management of Change workflow starts to check in or check out a file or binder associated with the selected asset, you can revert the Management of Change workflow status of the file and binder to the Initiated Check-in Workflow, Completed Check-in Workflow, Initiated Check-out Workflow, or Completed Check-out Workflow status.
Prerequisites
- To unblock a workflow, you must have theUnblock MoC workflowpermission.
To unblock a Management of Change workflow
- OnAssets, expand the asset tree, and then select a file or binder associated with the selected asset that is in the Management of Change workflow.
- Select theUnblock Workflowbutton.
- Complete theUnblock Workflowdialog.
- SelectOK.
Provide Feedback