Pen object

Member of the Pens collection.
The Pen object represents a pen on a trend. It is a member of the Pens collection.
Set up pens by using the Pen object properties or the Pens tab on the Trend properties dialog box.
Use the
Item
method of the Pens collection to get a reference to a Pen object.
The Pen object supports the following properties:
The Pen object supports the following method:
The Pen object supports the following constants:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal