CurrentScaleMax property

Returns the current maximum value by which the line is being scaled. The value depends on the scaling options and if the chart is zoomed. Read-only. Single.
Syntax
pen
.
CurrentScaleMax
where
pen
- is a Pen object or an expression that evaluates to a Pen object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal