Trend object

The Trend object represents a Trend object on a display.
The Trend object is not a creatable object. Trend objects are accessible via an Elements collection and as properties of the Display object.
The Trend object's properties and methods listed are available in VBA.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal