Style property
Returns or sets the line style for the pen. Read/write. Constant.
Line styles only apply to lines that have a width of 1. Wider lines are always solid.
Syntax
pen
.Style
[ = lineStyle
]where
pen
- is a Pen object or an expression that evaluates to a Pen object.lineStyle
- is a constant of the type RSTlineStyles that specifies the style the pen's line will be drawn in.Remarks
Visual Basic5 offers a Quick List feature to display a list of what may appear at an insertion point, for example,
My Pen.Style =
If you place the insertion point after the = sign and press Ctrl and Spacebar, a list of line styles appears.
Provide Feedback