CurrentScaleMin property
Returns the current minimum value by which the line is being scaled. The value depends on the scaling options and if the chart is zoomed. Read-only. Single.
Syntax
pen
.CurrentScaleMin
where
pen
- is a Pen object or an expression that evaluates to a Pen object.Provide Feedback