Example: Range
Private Sub SetRange() With Trend1 With .Pens.Item(1) .Min = -100 .Max = 100 End With With .YAxis ' Use the pen's min/max values. .MinMaxOption = rstPresetMinMax ' Use a separate range for each pen. .ScalingOption = rstLineScale 'Show the YAxis labels, which include the min and max .DisplayScale = True End With End With End Sub
Provide Feedback