Description property (Trend object)
Returns or sets the text description of a pen on a trend chart. Read/write. String.
If the DisplayLineLegend property is True, the description can appear on the chart as the pen caption in the line legend.
Syntax
pen
.Description
[ = text
]where
pen
- is a Pen object or an expression that evaluates to a Pen object.text
- is a parameter of the type String that describes the pen.Remarks
Operators can change the description at runtime by double-clicking the description in the line legend, if the RuntimeAttributesEnabled property is set to rstEnableEditLegend.
Chart example

Set up line legend options on the Trend properties Display tab.
Double-click the line legend at runtime to open the Pens tab. (This option must be selected on the Runtime tab.)
Provide Feedback