DisplayLineLegend property

Returns or sets whether or not to display a legend for each trend line on the chart. Read/write. Boolean.
Syntax
Trend
.
DisplayLineLegend
[ = state
]
where
Trend
- is the name of a Trend object (such as trend1) or an expression that evaluates to a Trend object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    . Displays the line legend.
  • False
    . Does not display the line legend.
Chart example
tx_LineLegend
Set up line legend options on the Trend properties Display tab.
Double-click the line legend at runtime to open the Pens tab. (This option must be selected on the Runtime tab.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal