LogScale property

Returns or sets whether the pen is shown with the logarithmic scale to base 10. Read/write. Boolean.
This property only works for standard chart style. When this property is enabled, the properties NumGridLines, NumMinorGridLines, and ScaleAsPercent of YAxis object are ignored.
Syntax
pen
.
LogScale
[
= state
]
where
pen
- is a Pen object or an expression that evaluates to a Pen object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    . Shows the pen with the logarithmic scale to base 10.
  • False
    . Shows the pen with the actual values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal