LinkData property

Returns or sets whether the pen's description, units, min and max are read from the source data item when the object is instantiated. Read/write. Boolean.
When LinkData is enabled, the corresponding pen properties (description, units, min and max) are read-only.
Syntax
pen
.
LinkData
[
= state
where
pen
- is a Pen object or an expression that evaluates to a Pen object.
state
- is a parameter of the type Boolean that can be set to one of the following:
  • True
    . Read the pen properties from the source data item.
  • False
    . Use the pen properties configured in the Pens tab of the Trend Properties dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal