Pens tab

Use the
Pens
tab to set up the color, line style, markers, and other attributes for each pen.
The pen attributes define how the tag for each pen will be represented on the runtime chart.
TIP:
To see all of the available attributes, use the scroll bar at the bottom of the
Pen Attributes
spreadsheet on the
Pens
tab.
The Trend objects cannot get the oldest data from the FactoryTalk Historian server when you click the Oldest Data button.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal