Add a pen from a data log model

Use the
Pens
tab to add a pen from a data log model.
To add a pen from a data log model:
  1. From the
    Pens
    tab, select
    DataLog Model
    from the
    Pen Source
    list.
  2. Click
    Add Pen(s)
    .
  3. From the
    Configure Tags
    dialog box, the home area is automatically selected. Click the browse button to select another area.
  4. From the list of data log models, select one data log model. The data log model tags are listed in the box below the model name.
  5. Click tags from the model to select them for the trend, and then click
    Add
    to add them to the
    Tags to monitor
    list.
  6. Click
    OK
    when all the tags to be in the monitored are selected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal