Apply attributes to multiple pens
Use the
Pens
tab to apply attributes to multiple pens.To apply attributes to multiple pens:
- Select multiple pens in thePen Attributesspreadsheet by pressing and holding theCtrlkey while clicking the tag names.
- In theMultiple Pen Editsbox, specify the attributes you want to apply to all of the selected pens, and then clickApply to Selected Pens.TIP:Making a snapshot available as an overlay also adds configurable pens to the trend.
Provide Feedback