Search
FactoryTalk View SE Help
Delete a pen
Use the
Pen Attributes
spreadsheet on the
Pens
tab to delete a pen.
To delete a pen from the trend:
In the
Pen attributes
spreadsheet, click the pen number, and then click
Delete Pen(s)
.
Pens tab
Add a new pen and set up its attributes
Add a pen from a data log model
Add a pen from a FactoryTalk Historian server
Apply attributes to multiple pens
Options in the Pen Attributes spreadsheet
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal