Logarithmic scale

A logarithmic scale is a scale of measurement that uses the logarithm of a physical quantity instead of the quantity itself. On a logarithmic scale, each tick mark on the scale is the previous tick mark multiplied by 10 when selected for a TrendX pen. The logarithmic scale can be helpful when the data covers a large range of values – the logarithm reduces this to a more manageable range.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal