Create a trend object
Create a trend object to show real-time data, and data from
FactoryTalk View SE
data logs.To create a trend object:
- Create or open a display in theGraphicseditor.
- From theObjectmenu, selectAdvanced > Trend.
- Drag the mouse to create a box approximately the size the trend chart is to be, and theTrend Propertiesdialog box opens.
- On the tabs in theTrend Propertiesdialog box, specify how the trend chart looks, how it works at runtime, the pens to use on trend, the horizontal axis and vertical axis, and the tags or expressions to plot.
Provide Feedback