X-Axis tab
Use the
X-Axix
tab to set up the time range and display options for the chart's runtime horizontal axis. The horizontal axis represents time for a standard line chart or the selected pen value for an xy plot.Provide Feedback