Runtime tab

Use this tab to determine which trend options are available to operators at runtime. To prevent operators from changing these options, the
Runtime
tab is not available at runtime.
You cannot work with the
Runtime
tab while a the trend is running. You need to be in edit mode. If you do not see the
Runtime
tab in the Trend property tabs, exit runtime mode and return to edit display mode.
The
Ctrl+Up Arrow
,
Ctrl+Down Arrow
,
Ctrl+Left Arrow
, and
Ctrl+Right Arrow
key combinations are reserved in
FactoryTalk View
SE, and cannot be used at runtime to pan a trend. Other directional keys and key combinations will work.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal