Template tab

Use this tab to save the settings for the current trend as a template, to load another template for the current trend to use, or to delete a template. The settings that are saved for the template are those from the
General
,
Display
,
Pens
, and
X
and
Y
Axis tabs.
A template can be applied to all trends in an application to create a consistent appearance. When you load a template, the property settings selected for the template are applied to the current trend and will be evident on the runtime chart.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal