Create a template (Trend)

Use the
Template
tab to create a template.
To create a template:
  1. Create a trend.
  2. On the
    Template
    tab, click a tab name on the left-hand side of the
    Select template options
    box.
  3. On the right side of the box, select the options available from that tab that are to be included in the template you are creating.
    Clear the check boxes for those options that should not included in the template.
  4. Repeat this process for all the tabs that are listed on the left-hand side.
  5. Click the
    Save Template
    button.
  6. Type a component name for the template and then click
    OK
    .
    The new template is saved immediately; it is not necessary to click
    OK
    , or
    Apply
    on the property tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal