Using keys in graphic animation
You can associate FactoryTalk View commands with graphic objects in a display, or with the display itself, using object keys and display keys.
A key can be either a key on a keyboard or keypad, or a button on a touch screen connected to the computer or monitor an operator is using to interact with an application at runtime.
Provide Feedback