Test display keys from the Graphics editor

You can test display keys from the graphics editor at runtime or in Test Display mode at design time.
To test the display keys from the Graphics editor:
  1. Click
    View
    >
    Test Display
    to activate the display that has focus.
  2. While the display is running, perform an action (press, hold, or repeat) for a key or key sequence, to test it.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal