Set up display key animation
Use the
Add Key
dialog box to define a display key.
TIP:
Repeat actions should be commands that change tag values. Actions that require user input or take a long time to run, can have unexpected results.
If a key action is to perform a task such as running a macro, use the press or release action.
To define a display key:
- In theGraphicseditor, right-click in a display and then clickDisplay Keys.
- In theDisplay Keysdialog box, clickAdd.
- In theAdd Keydialog box, in theKeyfield, click the down arrow to scroll the list and then click a key.
- In theModifiersbox, select theControlorShiftcheck box, or both, to create a key sequence, if required.
- In theDisplay Keysdialog box specify a label and press, repeat, or release actions, or a combination of actions, for the key.
- Click the browse button(...)beside an action field, to open theCommandwizard and use it to build a command string for the action.
Provide Feedback