Options in the Display Keys dialog box

The following table shows options in the
Display Keys
dialog box.
Options
Description
Label
Type a label that will be displayed in the key list. If you leave this blank, only the key or key sequence is displayed.
Press Action
A press action is carried out when the key, or key sequence, is pressed. Type the macro or command that will perform the action you require. To specify more than one command, separate the commands with a semicolon.
Repeat Action
A repeat action is carried out multiple times when the key, or key sequence, is pressed and held. The action is repeated at the rate specified in Windows Control Panel > Keyboard Properties.
Release Action
A release action is carried out when the key, or key sequence, is pressed and released. Type the macro or command that will perform the action you require.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal