Add Key or Modify Key dialog box
How do I open the Add Key or Modify Key dialog box
In the
Object Keys
dialog box, click Add
to open the Add Key
dialog box, or select a key and click Modify
to open the Modify Key
dialog box.You can add a object or display key in the Add Key dialog box. You can also modify an existing object or display key in the Modify Key dialog box.
The following table shows options in the
Add Key
or Modify Key
dialog box.Options | Description |
---|---|
Key | Click the down arrow to display the list of keys that can be used, then select the key that you want to attach to the object or display. |
Modifier | Select the Control or Shift check box, or both, to use a key modifier. |
Provide Feedback