Activate an object key

You can active the object key after it is defined.
To activate an object key:
  1. In FactoryTalk View Studio, on a graphic display, click
    View
    >
    Test Display
    .
  2. On the graphic display, click the object to show the list.
  3. In the list, click the object key definition that is to be activated.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal