Configure a local log destination

Use
Destination Setup
to configure settings for the local log installed on this computer. These options affect the single local log on this computer that any number of
FactoryTalk
products and services may be using.
In
Diagnostics Configuration
, select the plus (
+
) sign next to
Destination Setup
in the tree view on the left to display the current
FactoryTalk
logging destinations.
Local log destination items include:
  • Logging path
  • Maximum log size
  • Log overwrite options
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal