FactoryTalk Diagnostics Setup Help

FactoryTalk®
Diagnostics helps answer the question, "Why did that happen?"
FactoryTalk® Diagnostics
collects and provides access to a global store of time-and-date stamped messages.
The
FactoryTalk Diagnostics
service includes a Diagnostics Setup editor, a Diagnostics Viewer, and a local log on each computer where the
FactoryTalk® Services Platform
is installed. Other custom logging destinations are also available. For example, the
FactoryTalk® AssetCentre
software product provides customized
FactoryTalk
audit logs.
To set up options for logging destinations and to filter the types of messages logged on the local computer, use
Diagnostics Setup
.
To review diagnostics messages, use the
Diagnostics Viewer
. Diagnostics Viewer can be used to view both local messages and messages retrieved from logs on multiple computers.
FT_DIAG_Overview2
FactoryTalk View SE
,
FactoryTalk Alarms and Events
, and other
FactoryTalk
software products can send messages to both the local log and the
FactoryTalk
audit log on one computer. When settings options for a particular logging destination, the options affect the log on this computer that any number of
FactoryTalk
products may be using. Likewise, when configuring message routing options, the filtering options selected affect the types of messages routed from all
FactoryTalk
products that send messages to that destination.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal