FactoryTalk Diagnostics Setup

How do I run
FactoryTalk Diagnostics
Setup?
From the
Tools
menu, choose
FactoryTalk Diagnostics > Setup
.
Use the
FactoryTalk Diagnostics
Setup
to configure settings for each
FactoryTalk Diagnostics
logging destination installed on your computer. Configure these settings separately for each log on each computer where
FactoryTalk Diagnostics
is installed.
To configure settings for the local log or ODBC database, use
Destination Setup
.
Beginning with FactoryTalk Services Platform v6.50.00, FactoryTalk Diagnostics setup is changing to a centrally managed capability. The syslog destination is the initial capability exhibiting this change. To configure settings for the syslog destination, in the FactoryTalk Administration Console
Explorer
pane, go to
System > Policies > System Policies > FactoryTalk Diagnostics
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal