Route messages to logging destinations
Use
Message Routing
to configure the messages sent to specified logging destinations. This allows you to filter the messages by both audience and severity. For example, if you were only interested in receiving high priority messages classified by a particular FactoryTalk product or service as of high importance to software developers, you could configure your local log to log only "Error-Developer" and "Warning-Developer" messages, and to ignore all other messages. The "Secure" category of messages is reserved for audit messages that are logged by the
FactoryTalk AssetCentre
software. To route messages to logging destinations
- InMessage Routing, select one or more logging destinations from the window at left.
- Select check boxes in theMessage categoriesmatrix at right to select each message category to be routed to the destinations you have selected. Each message category is a pair: an audience, and a severity.
- IfFactoryTalk Diagnosticssupport forMicrosoftWindowsCE devices is installed on your computer, to accept CE-based messages, check the box markedAccept message from Windows CE devices or MobileView.
- SelectApply.
- Select another logging destination to configure, or selectOK.
Provide Feedback