Message Routing
How do I open Message Routing?
- From theFactoryTalk Administration ConsoleToolsmenu, chooseFactoryTalk Diagnostics Setup.
- From the Diagnostics Setup pane, clickMessage Routing.
Use
Message Routing
to specify which categories of messages should be routed to each logging destination available on your computer. Select one or more logging destinations from the left window. Next, select the boxes in the
Message categories
matrix to choose the type of messages that will be routed to the selected destinations. A message category consists of a severity option (such as Error) and an audience option (such as Engineer). The Secure category is reserved for audit messages and cannot be configured without FactoryTalk AssetCentre
installed on the system.Additionally, configure the selected logging destinations to accept messages from
PanelView Plus
or MobileView
. Provide Feedback