ODBC Database Destination Setup

How do I open ODBC Database Destination Setup?
  • From the left pane, open
    Destination Setup
    , then click
    ODBC Log
    .
Use
ODBC Database Destination Setup
to send messages to an ODBC data source. To send messages from multiple computers, configure the destination on each computer where the
FactoryTalk Diagnostics
service is installed.
Use
ODBC Database Destination Setup
to perform the following:
  • Set message buffering options
  • Select the ODBC data source
  • Create a new ODBC data source
  • Select or create a target table within the ODBC data source
  • Specify how log to maintain the connection to the database
  • Specify login settings
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal