Create a new ODBC data source

Use
ODBC Database Destination Setup
to create a new data source. You may create a file data source, user data source, or system data source.
TIP:
Alternatively, you may use
ODBC Database Destination Setup
to specify an existing ODBC file or system data source.
To create a new ODBC data source
  1. Under
    ODBC Data Source
    , next to
    Data source name
    , select
    Browse (...)
    .
  2. In
    Select Data Source,
    select
    New
    .
  3. Follow the instructions in the
    Create New Data Source
    wizard to create the new data source.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal