Configure an ODBC database log destination
Use
ODBC Database Destination Setup
to send messages to an ODBC data source. To send messages from multiple computers, configure the destination on each computer where the FactoryTalk Diagnostics
service is installed. FactoryTalk Diagnostics cannot log to a remote database using Microsoft Access. You can only log to a local database using Microsoft Access.The ODBC Database destination supports these ODBC-compliant databases:
- Microsoft®SQL Server®
- Access®
- Oracle®
Some types of information cannot be logged to an ODBC database destination. These include:
- Any additional database fields not included in the ODBC table format that aFactoryTalkproduct might use. Even if you create the additional fields manually, nothing will be logged to them. The additional information logged by aFactoryTalkproduct will, however, appear in the local log on the computer where the product is installed. See documentation for the products you are using to determine whether they make use of additional fields.
- Any messages where the audience type is set toSecure, or the severity type set toAudit. Secure messages can only be logged by the FactoryTalk AssetCentre software product to the FactoryTalk Audit Log.
Provide Feedback