Set ODBC database connection time

Use
ODBC Database Destination Setup
to specify the length of time that the system will remain connected to the ODBC database.
To set the ODBC database connection time
  1. From the left pane, open
    Destination Setup
    , then select
    ODBC Log
    .
  2. Under
    ODBC Data Source
    , to the right of
    Maintain connection
    , select one of the following:
    • for __ minutes
    • indefinitely
  3. (optional) Enter the number of minutes the ODBC database remains connected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal