Select an ODBC data source

Use
ODBC Database Destination Setup
to select an ODBC data source.
TIP:
Alternatively, you may use
ODBC Database Destination Setup
to create a new ODBC data source.
To select an ODBC data source
  1. Under
    ODBC Data Source
    , next to
    Data source name
    , type the path and file name of a system or file ODBC data source, or select
    Browse (...)
    to browse for an existing data source.
    If using
    Browse
    , the
    Select Data Source
    dialog box displays which lists the file and system data sources available on the computer where
    FactoryTalk Diagnostics
    is running.
    Either:
    1. Select a file data source
      • On the
        File Data Source
        tab,
        next to
        Look in:
        , select
        Browse (...)
        .
      • In
        Browse for Folder
        select a folder in which to search for an ODBC File data source. Select any file data source that refers to an ODBC driver installed on the local computer and select
        OK.
    2. Select a system data source
      • On the
        System Data Source
        tab, select one of the files listed.
  2. Select
    OK
    to return to
    ODBC Database Destination Setup
    .
    TIP:
    Beginning with
    FactoryTalk Services Platform
    version 6.30, the
    Log On
    account of
    FactoryTalk Diagnostics
    Local Reader
    service has been changed to a
    Local Service
    account. Due to permission limitations, the
    Local Service
    account may not have read access to the
    Data Source
    folder. Once you have selected a data source file and folder, and click
    OK
    , a warning message may show, asking whether you want to grant the
    Local Service
    account read permission for the selected folder. Select
    Yes
    to continue using the folder and grant read permission to the
    Local Service
    account. Select
    No
    to choose another folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal