Local Log Destination Setup
How do I open Local Log
Destination Setup?
- From theFactoryTalk Administration ConsoleToolsmenu, chooseFactoryTalk Diagnostics > Setup.
- If prompted byWindowsUser Account Control to allow the application to make changes, selectedYes.
- In theDiagnostics Configurationwindow, expandDestination Setup, and then selectLocal Log.
Use
Local Log Destination Setup
to configure settings for the local log installed on this computer.
TIP:
- If the default destination for the Local Log file in the Logging path is changed, restart the computer for the new file location to be detected.
- The Local Log default location is%SystemRoot%\system32\winevt\Logs.
These settings affect the single local log on this computer that any number of
FactoryTalk
products and services may be using.Setting | Description |
|---|---|
Logging path | Identifies the location of the FactoryTalk Diagnostics local log on this computer. To change the log location, select Browse to locate the new folder. Reboot the machine for the new file location to be detected. |
Maximum log size | Enter the maximum size of the log file, in KB, that you want to store. The overwrite options specify what happens when the maximum log size is reached. The minimum log size is 1028 KB. Use the up or down buttons to change the maximum log size in increments of 64K. If a value is entered or selected that is not a multiple of 64, the log size is set to the nearest multiple of 64. |
When maximum log size is reached: | Choose an option to control what happens if the log file reaches its maximum size limit:
|
Clear Log | Permanently deletes all events from the log. Provides an option to save the logged events to a file. |
Provide Feedback