Configure a logging destination to refuse PanelView Plus and MobileView messages

Use
Destination Setup
to disable the computer's ability to receive messages broadcast from
PanelView Plus
and
MobileView
devices.
To configure a logging destination to refuse
PanelView Plus
and
MobileView
messages
  1. In
    Diagnostics Configuration
    , select
    Destination Setup
    .
  2. Clear
    Enable this computer to receive messages broadcast from
    PanelView Plus
    or
    MobileView
    .
    This prevents messages generated from
    PanelView Plus
    and
    MobileView
    from being routed to the computer for logging.
  3. On
    Message Routing,
    configure each logging destination to not accept messages from
    PanelView Plus
    and
    MobileView
    .
  4. If editing other settings in Diagnostics Setup, select
    Apply
    to save the new destination message routing setup. When finished making changes in
    Diagnostics Configuration
    , select
    OK
    to close the window.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal