Configure a logging destination to accept PanelView Plus and MobileView messages
Use
Destination Setup
to enable the computer's ability to receive messages broadcast from PanelView Plus
and MobileView
devices. To configure a logging destination to accept
PanelView Plus
and MobileView
messages- InDiagnostics Configuration, selectDestination Setup.
- SelectEnable this computer to receive messages broadcast fromto route messages generated fromPanelView PlusorMobileViewPanelView PlusorMobileViewto the computer for logging.FactoryTalk DiagnosticsroutesPanelView Plusmessages based on the standard "audience" and "severity" categories assigned to each message.
- (optional) Enter a value in thePortfield if your devices are using custom port values. Typically, do not change the default port setting. The Port value on this computer and the Port value set in thePanelView Plusdevice's registry must match for the two computers to communicate.
- SelectMessage Routing
- Select a logging destination that needs to accept messages fromPanelView PlusorMobileView.
- SelectAccept message fromPanelView PlusorMobileView.Repeat as needed for each logging destination.
- If editing other settings in Diagnostics Setup, selectApplyto save the new destination message routing setup. When finished making changes inDiagnostics Configuration, selectOKto close the window.
Provide Feedback